TCPIP_SNTP_EVENT Enumeration
C
typedef enum {
TCPIP_SNTP_EVENT_NONE = 0,
TCPIP_SNTP_EVENT_TSTAMP_OK = 1,
TCPIP_SNTP_EVENT_DNS_ERROR = -1,
TCPIP_SNTP_EVENT_IF_ERROR = -2,
TCPIP_SNTP_EVENT_SKT_ERROR = -3,
TCPIP_SNTP_EVENT_SERVER_TMO = -4,
TCPIP_SNTP_EVENT_VER_ERROR = -5,
TCPIP_SNTP_EVENT_TSTAMP_ERROR = -6,
TCPIP_SNTP_EVENT_KOD_ERROR = -7,
TCPIP_SNTP_EVENT_SYNC_ERROR = -8
} TCPIP_SNTP_EVENT;
Description
Provides a list of run time SNTP events.
Members
Members | Description |
---|---|
TCPIP_SNTP_EVENT_NONE = 0 | Invalid event success. |
TCPIP_SNTP_EVENT_TSTAMP_OK = 1 | A new NTP timestamp has been acquired successfully. |
TCPIP_SNTP_EVENT_DNS_ERROR = -1 | NTP server name DNS failed. |
TCPIP_SNTP_EVENT_IF_ERROR = -2 | Could not select a valid NTP interface. |
TCPIP_SNTP_EVENT_SKT_ERROR = -3 | Could not bind the socket to the NTP interface or timeout on the socket TX. |
TCPIP_SNTP_EVENT_SERVER_TMO = -4 | No reply received from the NTP server. |
TCPIP_SNTP_EVENT_VER_ERROR = -5 | The server response has a wrong version. |
TCPIP_SNTP_EVENT_TSTAMP_ERROR = -6 | The server response had a wrong timestamp. |
TCPIP_SNTP_EVENT_KOD_ERROR = -7 | The server replied with a "Kiss O' Death" code. |
TCPIP_SNTP_EVENT_SYNC_ERROR = -8 | The server response has a synchronization error. |