11.3.2 Writing to DFM
To write a DFM location, the address must first be written to the NVMADR register and the data written to the NVMDATL register. The sequence shown in 11.1.2 NVM Unlock Sequence must be followed to initiate the write cycle. Block writes, also referred to as sector writes, are not supported for the DFM.
The write will not begin if NVM Unlock sequence is not exactly followed for each byte. It is strongly recommended that interrupts be disabled during this code segment.
Additionally, the NVMEN bit must be set to enable NVM control. This mechanism prevents accidental writes to DFM due to unexpected code execution (i.e., runaway programs). The NVMEN bit should be kept clear at all times, except when updating the DFM. The NVMEN bit is not cleared by hardware.
After a write sequence has been initiated, NVMCON1, NVMADR and NVMDAT cannot be modified. The WR bit will be inhibited from being set unless the NVMEN bit is set.
After a write sequence has been initiated, clearing the NVMEN bit will not affect this write cycle. A single DFM byte is written and the operation includes an implicit erase cycle for that word. CPU execution continues in parallel and at the completion of the write cycle, the WR bit is cleared in hardware and the NVM Interrupt Flag bit (NVMIF) is set. The user can either enable this interrupt or poll this bit. NVMIF must be cleared by software.
DFM Write
; Data Flash Memory Address to write
MOVF DFM_ADDRL, W ;
MOVWF NVMADRL ; Setup Address low byte
MOVF DFM_ADDRH, W ;
MOVWF NVMADRH ; Setup Address high byte
MOVF DFM_ADDRU, W ;
MOVWF NVMADRU ; Setup Address upper byte
; Data Memory Value to write
MOVF DMF_DATA, W ;
MOVWF NVMDATL ;
; Enable writes
BSF NVMCON0, NVMEN ; Enable NVM
; Disable interrupts
BCF INTCON, GIE ;
; –------- Required Sequence –--------
MOVLW 55h ;
MOVWF NVMCON2 ;
MOVLW AAh ;
MOVWF NVMCON2 ;
BSF NVMCON1, WR ; Set WR bit to begin write
; –------------------------------------
; Wait for write to complete
BTFSC NVMCON1, WR ; DFM writes do not stall the CPU
BRA $-2
; Enable INT
BSF INTCON, GIE ;
; Disable writes
BCF NVMCON0, NVMEN ;