24.7.2 Dead-Band Functionality in Full-Bridge mode
In Full-Bridge mode, the dead-band counters are used when undergoing a direction change. The MODE<0> bit can be set or cleared while the CWG is running, allowing for changes from Forward to Reverse mode. The CWGxA and CWGxC signals will change immediately upon the first rising input edge following a direction change, but the modulated signals (CWGxB or CWGxD, depending on the direction of the change) will experience a delay dictated by the dead-band counters.