4.1 Libero
The following table lists known issues and limitations associated with Libero SoC v2021.3.
| Family | Description |
|---|---|
| PolarFire and PolarFire SoC | Non-recoverable zeroization mode is not programmed with Libero design, which does not have any POR digest configured and no custom security. |
| All | The vdir command used with ModelSim ME Pro 2021.3 for
pre-compiled libraries on v2021.3 delivers the incorrect result of unknown
version. |
| PolarFire |
Simulations fail for system services when they look for
Workaround: Rename |
| N/A | Identify debugger 2021-03M with Libero 2021.2 crashes on 11th generation Windows 10 machines. |
| SmartFusion2 | Synthesis error occurs when trying to open encrypted HDL files on 11th generation Windows 10 machines. |
| IGLOO2, SmartFusion2 and RTG4 | When the FDDR/MDDR is configured to support 4GB, it cannot access the entire 32-bit AXI address range. Designs that do not map the MSB of the 32-bit AXI address to the DDR memory address are not affected (that is, if the AXI address does not exceed a 2GB address space). |
| PolarFire | In the PolarFire DDR4 Configurator, users can enable both ECC and DM at the same time. These should be mutually exclusive selections. |
| PolarFire | Signal integrity settings from I/O editor have no effect on design implementation in Libero 2021.3. |
| IGLOO2 |
When all the keys ( The action 'ERASE' is not supported. You must select the programming action from this list: 'DEVICE_INFO, ENC_DATA_AUTHENTICATION, PROGRAM, READ_DEVICE_CERTIFICATE, READ_IDCODE'. The action 'VERIFY' is not supported. You must select the programming action from this list: 'DEVICE_INFO, ENC_DATA_AUTHENTICATION, PROGRAM, READ_DEVICE_CERTIFICATE, READ_IDCODE'.
Workaround: Do not run ERASE and VERIFY actions when all the keys
( |
| PolarFire | Incorrect PUFT timing is reported when SPI Flash is using as an Initialization client. |
| All |
If an Identify implementation was created through Libero project before another
synthesis implementation ( Workaround: Whenever Identify implementation is created through Libero -> Synthesis -> Configure Options, open SynplifyPro interactively, instrument the design, and run synthesis before running any synthesis or creating new implementation. Then return to Libero and create a new synthesis/identify implementation. |
| RTG4 |
When the Hold output in reset (output low) after power-up. Released and
resynchronized with the PLL reference clock after the PLL locked
option is set for the RTG4FCCCECALIB core, the clock appears at the output before
the
Workaround: When synchronizer is used for the |
| All |
In Libero flow, when multiple identify implementations are created and run initially, an error message appears only in the synthesis log, but does not propagate to the Libero error log. The following error message appears in the Libero window: No instrumentation file found for Identify implementation. Please open SynplifyPro interactively to launch Identify Instrumentor |
| PolarFire |
The following enhancement to Synthesis Compiler in this SynplfiyPro 2020.09MSp1
release (Libero v2021.1 release) is related to the initial value support for memory
initialization and is not technology specific. Test cases with the MiV core fails in
synthesis with the following error message:
:"./component/work/MIV_RV32IMA_L1_AXI_C0/MIV_RV32IMA_L1_AXI_C0_0/core/miv_rv32ima_l1_axi_data_arrays_0_ext.v":81:24:81:38|Loop iteration limit 2000 exceeded - add '// synthesis loop_limit 4000' before the loop construct Workaround: In the Libero graphical user interface, select the Synthesis > Configure Option > Additional Parameters box and set_option -looplimit 4000 OR Add the following configure_tool -name {SYNTHESIZE} -params {BLOCK_MODE:false} -params {BLOCK_PLACEMENT_CONFLICTS:ERROR} -params {BLOCK_ROUTING_CONFLICTS:LOCK} -params {CLOCK_ASYNC:800} -params {CLOCK_DATA:5000} -params {CLOCK_GLOBAL:2} -params {PA4_GB_COUNT:24} -params {PA4_GB_MAX_RCLKINT_INSERTION:16} -params {PA4_GB_MIN_GB_FANOUT_TO_USE_RCLKINT:1000} -params {RAM_OPTIMIZED_FOR_POWER:0} -params {RETIMING:false} -params {SEQSHIFT_TO_URAM:0} -params {SYNPLIFY_OPTIONS: set_option -looplimit 4000} -params {SYNPLIFY_TCL_FILE:}
|
| ALL | If a module is present in an include file, the file appears as a linked file inside the project. If there is a broken Global Include Path for such projects, the include file is also shown with a broken link. If the project is closed and re-created, the correct Global Include Path appears properly. If the Global Include path under Project Settings is changed, two links are shown for include file inside the project: one with the new Global Include Path as shown inside the project, and another that is the broken link with the previous Global Include Path. There is no issue with functionality, but an extra broken link is shown in the project. Remove this link when the Global Include Path in Project Settings is changed. |
| RTG4 and PolarFire |
I/O Editor shows resistor pull for P and N pins when LVDS failsafe (Dynamic ODT) is enabled. For RTG4 and PolarFire families, the resistor pull information for P and N pins are shown as pull up or both as pull down. They should be pull up for one pin and pull down for the other pin. This is a display issue only that existed in the I/O Editor and the pin report since 11.9 SP3. Due to a software infrastructure limitation, the P and N sides cannot have different values. Regardless of the display issue, both P and N sides program correctly:
|