6.4 GenDivKey Command
The GenDivKey command is used to generate the diversified key that is equivalent to the one programmed into the SHA104 or other client-side device. The command is similar to the GenDig command of other CryptoAuthentication devices but is much more limited in scope.
This command only makes sense to run when using a system with diversified keys. Upon completion, the value of the client side diversified key will be loaded into TempKey for use by the CheckMac command.