11.3.3.3 bss [DD]
The bss attribute specifies that a section should be allocated as uninitialized storage in data memory, as defined by region data in the linker script. The following attributes may be used in conjunction with bss and will further specify the allocation:
address()specifies an absolute addressnearspecifies the first 8K of data memoryxmemory[DD] specifies X address space, which includes all of region data below the address __YDATA_BASE as defined in the linker script (dsPIC30F/33F DSCs only)ymemory[DD] specifies Y address space, which includes all of region data above the address __YDATA_BASE as defined in the linker script (dsPIC30F/33F DSCs only)align()specifies alignment of the section starting addressreverse()specifies alignment of the section ending address + 1dma[DD] specifies dma address space, which includes the portion of region data between addresses __DMA_BASE and __DMA_END as defined in the linker script (dsPIC33F DSCs only).bootspecifies the boot segmentsecurespecifies the secure segment