11.3.3.1 code

The code attribute specifies that a section should be allocated in program memory, as defined by region program in the linker script. The following attributes may be used in conjunction with code and will further specify the allocation:

  • address() specifies an absolute address
  • align() specifies alignment of the section starting address
  • boot specifies the boot segment
  • secure specifies the secure segment