11.3.3.6 memory
The memory attribute specifies that a section should be allocated in external or user-defined memory. The following attributes may be used in conjunction with memory and will further specify the allocation:
address()specifies an absolute addressalign()specifies alignment of the section starting addressreverse()specifies alignment of the section ending address + 1noloadspecifies that the section should not be loaded with the primary applicationNote: Sections allocated in external or user-defined memory cannot be accessed by the PSV window or the EDS window.
eedata – dsPIC30F DSCs only [DD]
The eedata attribute specifies that a section should be allocated in data EEPROM memory, as defined by region eedata in the linker script. The following attributes may be used in conjunction with eedata and will further specify the allocation:
address()specifies an absolute addressalign()specifies alignment of the section starting addressreverse()specifies alignment of the section ending address + 1bootspecifies the boot segmentsecurespecifies the secure segment