11.3.3.1 code
The code attribute specifies that a section should be allocated in program memory, as defined by region program in the linker script. The following attributes may be used in conjunction with code and will further specify the allocation:
address()specifies an absolute addressalign()specifies alignment of the section starting addressbootspecifies the boot segmentsecurespecifies the secure segment