NAND Flash Boot: PMECC Error Detection and Correction
NAND Flash boot procedure uses PMECC to detect and correct errors during NAND Flash read operations in two cases:
- When the usePmecc flag is set in a specific NAND header. If the flag is not set, no ECC correction is performed during the NAND Flash page read.
- When the NAND Flash has been detected using ONFI parameters.
The ROM memory embeds the Galois field tables. The user does not need to embed them in his/her own software.
The Galois field tables are mapped in the ROM just after the ROM code, as shown in the following figure.
For a full description and an example of how to use the PMECC detection and correction feature, refer to the software package dedicated to this device on www.microchip.com.