4.2.4 Compilation of Assembly Source
Assembly source files that are part of a C project are compiled in a similar way to C source files. The compiler driver knows that these files should be passed to a different set of internal compiler applications and a single build command can contain a mix of C and assembly source files, as in the following example.
xc8-cc -mcpu=16F1946
-mdfp="Microchip/PIC12-16F1xxx_DFP/1.7.242/xc8" proj.c spi.s
If an assembly source file contains C preprocessor directives that must be preprocessed before passed to the assembler, then ensure the source file uses a .S extension, for example spi.S.
The compiler can be used to generate assembly files from C source code using the
-S option. The assembly output can then be used as the basis for your
own assembly routines and subsequently compiled using the command-line driver.
MPLAB XC8 builds assembly source files before C source files, so that information contained in the assembly code can be subsequently passed to the code generator, see Interaction between Assembly and C Code.
The intermediate file
format associated with assembly source files is an object file (.o
extension). The -c option (see C: Compile To Intermediate File) will halt compilation after the
assembly step when building assembly source files, generating the object file.