5.3.6.3.2 Pointer Classifications with Local Optimization
Where local optimizations have been enabled, pointers can have a size and classification based purely on their definition, not on the targets assigned to them by the program.
The pointer-target specifiers, __ram and
__rom, (see Pointer-target Qualifiers) can be used to ensure that addresses
assigned to a pointer during the program’s execution are within an intended memory space.
Together with a restricted range of pointer classifications, this ensures that pointers
will have a size that is predictable.
Pointers defined in code built with local optimizations and which have the indicated targets will have the following sizes, where type is a valid, unqualified C type.
const type *- can be assigned the address of any object in data or program memory. These pointers will be 3 bytes wide if the program is being built for a PIC18 device that has more than 64 KB of program memory; they will be 2 bytes wide, otherwise.
__rom type *- can be assigned the address of any object in program memory, and attempts to assign
the address of a data memory object will result in an error. These pointers will be 3
bytes wide if the program is being built for a PIC18 device that has more than 64 KB
of program memory; they will be 2 bytes wide, otherwise. The
constspecifier can be optionally used with__romwithout changing the pointer size. type *- can be assigned the address of any object in data memory. As per normal operation,
the compiler will issue a warning if the address of a
constobject is assigned to such pointers. These pointers are always 2 bytes in size. __ram type *- can be assigned the address of any object in data memory and attempts to
assign the address of a program memory object will result in an error. These pointers
will always be 2 bytes in size. The presence of the
constspecifier indicates only that the target objects must be treated as read-only. Theconstspecifier can be optionally used with__ramwithout changing the pointer size.
The size and operation of pointers to __far, pointers to
__eeprom, and function pointers are not affected by the local
optimization setting.