| “Any library facilities available to a
freestanding program, other than the minimal set required by clause 4
(5.1.2.1).” |
| See the compiler users guide relevant to your target device. |
“The format of the diagnostic printed by the
assert macro (7.2.1.1).” |
| Assertion failed: expression (file: func:
line) |
“The representation of floating-point exception
flags stored by the fegetexceptflag function
(7.6.2.2).” |
| Unimplemented. |
“Whether the feraiseexcept
function raises the inexact exception in addition to the overflow or underflow
exception (7.6.2.3).” |
| Unimplemented. |
“Strings other than "C" and
"" that may be passed as the second argument to the
setlocale function (7.11.1.1).” |
| None. |
“The types defined for float_t
and double_t when the value of the
FLT_EVAL_METHOD macro is less than 0 or greater than 2
(7.12).” |
| Unimplemented. |
| “Domain errors for the mathematics functions,
other than those required by this International Standard (7.12.1).” |
| None. |
| “The values returned by the mathematics functions
on domain errors (7.12.1).” |
| The errno variable is set to EDOM on
domain errors |
“Whether the mathematics functions set
errno to the value of the macro ERANGE on
overflow and/or underflow range errors (7.12.1).” |
| Yes |
“Whether a domain error occurs or zero is returned
when the fmod function has a second argument of zero
(7.12.10.1).” |
| The first argument is returned. |
“The base-2 logarithm of the modulus used by the
remquo function in reducing the quotient
(7.12.10.3).” |
| Unimplemented. |
“Whether the equivalent of signal(sig,
SIG_DFL); is executed prior to the call of a signal handler, and if
not, the blocking of signals that is performed (7.14.1.1).” |
| Signals are not implemented. |
“The null pointer constant to which the macro
NULL expands (7.17).” |
| ((void*)0) |
| “Whether the last line of a text stream requires a
terminating new-line character (7.19.2).” |
| Streams are not implemented. |
| “Whether space characters that are written out to
a text stream immediately before a new-line character appear when read in
(7.19.2).” |
| Streams are not implemented. |
| “The number of null characters that may be
appended to data written to a binary stream (7.19.2).” |
| Streams are not implemented. |
| “Whether the file position indicator of an
append-mode stream is initially positioned at the beginning or end of the file
(7.19.3).” |
| Streams are not implemented. |
| “Whether a write on a text stream causes the
associated file to be truncated beyond that point (7.19.3).” |
| Streams are not implemented. |
| “The characteristics of file buffering
(7.19.3).” |
| File handling is not implemented. |
| “Whether a zero-length file actually exists
(7.19.3).” |
| File handling is not implemented. |
| “The rules for composing valid file names
(7.19.3).” |
| File handling is not implemented. |
| “Whether the same file can be open multiple times
(7.19.3).” |
| File handling is not implemented. |
| “The nature and choice of encodings used for
multibyte characters in files (7.19.3).” |
| File handling is not implemented. |
| “The effect of the remove function on an open file
(7.19.4.1).” |
| File handling is not implemented. |
| “The effect if a file with the new name exists
prior to a call to the rename function (7.19.4.2).” |
| File handling is not implemented. |
| “Whether an open temporary file is removed upon
abnormal program termination (7.19.4.3).” |
| File handling is not implemented. |
“What happens when the tmpnam
function is called more than TMP_MAX times
(7.19.4.4).” |
| File handling is not implemented. |
| “Which changes of mode are permitted (if any) and
under what circumstances (7.19.5.4).” |
| File handling is not implemented. |
| “The style used to print an infinity or NaN and
the meaning of the n-char-sequence if that style is printed for a NaN
(7.19.6.1, 7.24.2.1).” |
| NaN is printed as nan, with no char sequence printed.
Infinity is printed as [-/+]inf. |
“The output for %p conversion in
the fprintf or fwprintf function (7.19.6.1,
7.24.2.1).” |
| Functionally equivalent to %lx. |
“The interpretation of a -
character that is neither the first nor the last character, nor the second
where a ^ character is the first, in the
scanlist for %[ conversion in the
fscanf or fwscanf function (7.19.6.2,
7.24.2.2).” |
| Streams are not implemented. |
“The set of sequences matched by the
%p conversion in the fscanf or
fwscanf function (7.19.6.2, 7.24.2.2).” |
| Streams are not implemented. |
“The value to which the macro
errno is set by the fgetpos,
fsetpos, or ftell functions on failure
(7.19.9.1, 7.19.9.3, 7.19.9.4).” |
| Streams are not implemented. |
“The meaning of the n-char-sequence in a string
converted by the strtod, strtof,
strtold, wcstod, wcstof,
or wcstold function (7.20.1.3, 7.24.4.1.1).” |
| No meaning is attached to the sequence. |
“Whether or not the strtod,
strtof, strtold, wcstod,
wcstof, or wcstold function sets
errno to ERANGE when underflow occurs
(7.20.1.3, 7.24.4.1.1).” |
| No. |
“Whether the calloc,
malloc and realloc functions return a Null
Pointer or a pointer to an allocated object when the size requested is zero
(7.20.3).” |
| The requested size is bumped to 1 byte. If this can be successfully
allocated, a pointer to the space is returned; otherwise NULL
is returned. |
| “Whether open output streams are flushed, open
streams are closed, or temporary files are removed when the abort function is
called (7.20.4.1).” |
| Streams are not implemented. |
| “The termination status returned to the host
environment by the abort function (7.20.4.1).” |
| The host environment is application defined. |
| “The value returned by the system function when
its argument is not a Null Pointer (7.20.4.5).” |
| The host environment is application defined. |
| “The local time zone and Daylight Saving Time
(7.23.1).” |
| Application defined. |
“The range and precision of times representable
in clock_t and time_t (7.23)” |
| The time_t type is used to hold a number of seconds and is
defined as a long type; clock_t is defined as
an unsigned long. |
| “The era for the clock function
(7.23.2.1).” |
| Application defined. |
“The replacement string for the
%Z specifier to the strftime,
strfxtime, wcsftime and
wcsfxtime functions in the "C" locale
(7.23.3.5, 7.23.3.6, 7.24.5.1, 7.24.5.2).” |
| These functions are not implemented. |
| “Whether or when the trigonometric, hyperbolic,
base- exponential, base- logarithmic, error and log gamma functions raise
the inexact exception in an IEC 60559 conformant implementation (F.9).” |
| No. |
“Whether the functions in
<math.h> honor the Rounding Direction mode
(F.9).” |
| The rounding mode is not forced. |