11.2 Translation
| ISO Standard | Implementation |
|---|---|
| “How a diagnostic is identified (3.10, 5.1.1.3).” | |
By default, when compiling on the command-line the following formats are
used. The string (warning) is only displayed for warning
messages.or where
| |
| “Whether each nonempty sequence of white-space characters other than new-line is retained or replaced by one space character in translation phase 3 (5.1.1.2).” | |
| The compiler will replace each leading or interleaved whitespace character sequences with a space. A trailing sequence of whitespace characters is replaced with a new-line. | |