5.1.3.2 Floating-point Types
The specification of the floating-point types, especially the
double and long double types can vary from that
mandated by the C standard. For example, the
DBL_DIG/LDBL_DIG macro values specified by
<float.h> are smaller than that indicated by the standard. Similarly
the DBL_EPSILON/LDBL_EPSILON macro values are larger than
that indicated by the standard.
These macros are listed in the Microchip Unified Standard Library Reference Guide.