5.4.3 Objects in Program Space
Variables with static storage duration and that are qualified const are
placed into program memory. Some auto objects might also be positioned there, as discussed
in Const Auto Objects. Note that some
optimizations (see Cacheconst Option)
attempt to cache const-qualified objects into data memory, where they are
accessed more efficiently.
Accessing data located in program memory is much slower than accessing objects in the data memory. The code associated with the access is also larger.
Enhanced Mid-range devices can directly read their program memory, although the compiler
will still usually store data as retlw instructions. This way the compiler
can either produce code that can call these instructions to obtain the program memory data
as with the ordinary Mid-range devices, or directly read the operand to the instruction
(the LSB of the retlw instruction). The most efficient access method can
be selected by the compiler when the data needs to be read.
Data can be stored as individual bytes in the program memory of PIC18 devices. This can be read using table read instructions. Note that the table pointer should not be manually modified during program execution. See Register Usage for more information.
EBTRx bits on
some PIC18 devices. If this protection feature is enabled, code might fail to read objects
stored in the blocks of program memory that have been protected. Ensure that program-memory
sections holding data are not unintentionally linked into protected program memory
blocks.For other 8-bit PIC devices, the program space is
not directly readable by the device. For these devices, the compiler stores data in the
program memory by means of retlw instructions which can be called and will
return a byte of data in the W register. The compiler will generate the code necessary to
make it appear that program memory is being read directly.