7.4.12 Function events_is_busy()
Check if a channel is busy.
bool events_is_busy( struct events_resource * resource)
Check if a channel is busy, a channel stays busy until all users connected to the channel has handled an event.
| Data direction | Parameter name | Description |
|---|---|---|
|
[in] |
resource |
Pointer to a events_resource struct instance |
Returns
Status of the channels busy state.
| Return value | Description |
|---|---|
|
true |
One or more users connected to the channel has not handled the last event |
|
false |
All users are ready to handle new events |