4.3.8.1 Const Type Qualifier
The const type qualifier is used to tell the compiler
that an object is read only and should not be modified. If any attempt is made to modify
an object declared const, the compiler will issue a warning or
error.
Provided that no other storage qualifiers are used,
const-qualified objects (excluding autos and parameters) are by
default linked into the program space, however this can be changed by using the
-mno-const-data-in-progmem option (see Const-data-in-progmem Option). Such
objects can also be made absolute, allowing them to be easily placed at a specific
address in the program memory, see Absolute Objects In Program Memory.
Objects qualified with const are accessed as if they
were qualified with __memx, see Memx Address Space Qualifier. If the definition
of const-qualified objects also uses storage qualifiers, such as
__flash or __flashn (see Flash Qualifier and Flashn Qualifiers) the read access
strategy implied by these qualifiers take precedence over that implied by
const.
Usually a const object must be initialized when it is
declared, as it cannot be assigned a value at any point at runtime. For example:
const int version = 3;
will define version as being a read-only
int variable, holding the value 3.