4.3.10.2 Address Attribute
The
address(addr) attribute is used to alias an
object identifier to a peripheral address that may lie outside the IO address range.
Such identifiers can then be used to address these memory-mapped peripherals. For
example:volatile int porta __attribute__((address (0x600)));will
internally equate porta to the address 0x600.This attribute does not affect the allocation of any ordinary object in memory. To place
objects at a specified address in the ordinary data memory, use the
__at() specifier (see Absolute Variables).