4.3.10.9 Persistent Attribute
The persistent attribute is used to indicate that
objects should not be cleared by the runtime startup code.
By default, C objects with static storage duration that are not
explicitly initialized are cleared on startup. This is consistent with the definition of
the C language. However, there are occasions where it is desirable for some data to be
preserved across a Reset. The persistent attribute stores objects with
static storage duration in a separate area of memory that is not altered by the runtime
startup code.
intvar and
mode are not cleared at
startup:int __attribute__((persistent)) mode;
void test(void)
{
static int __attribute__((persistent)) intvar; /* must be static in this context */
...
}<xc.h> header is included, a more
portable macro, __persistent, is available. For example, the following
CCI-compliant code is similar to the
above:#include <xc.h>
__persistent int mode;
void test(void)
{
static __persistent int intvar; /* must be static in this context */
...
}