37.3.6.4 Fast Point Doubling

Purpose

This service is used to perform a Point Doubling, based on a given elliptic curve over GF(p).

How to Use the Service

Description

These two services process the Point Doubling:

PtC = 2 × PtA

In this computation, the following parameters need to be provided:

  • A the input point is filled in projective coordinates (X,Y,Z) (pointed by {nu1PointABase,3*u2ModLength + 12}). This point can be the Infinite Point.
  • Cns the Fast Modular Constant filled (pointed by {nu1CnsBase,u2ModLength +8})
  • P the modulus filled (pointed by {nu1ModBase,u2ModLength +4})
  • The workspace not initialized (pointed by {nu1WorkSpace, 4*u2ModLength +28}
  • The a parameter relative to the elliptic curve (pointed by {nu1ABase,u2ModLength +4})
  • The resulting C point is represented in projective coordinates (X,Y,Z) and is stored at the same location than the input point A. This point can be the Infinite Point.

The service name for this operation is ZpEccDblFast. This service uses Fast mode and Fast Modular Reduction for computations.

Important: Before using this service, ensure that the constant Cns has been calculated with the setup of the Fast Modular Reduction service.

Parameters Definition

Table 37-72. ZpEccDblFastService
ParameterTypeDirectionLocationData LengthBefore Executing the ServiceAfter Executing the Service
nu1ModBasenu1ICrypto RAMu2ModLength + 4Base of modulus PBase of modulus P
nu1CnsBasenu1ICrypto RAMu2ModLength + 8Base of CnsBase of Cns
u2ModLengthu2ILength of modulus PLength of modulus P
nu1ABaseu2ICrypto RAMu2ModLength + 4Parameter a of the elliptic curveParameter a of the elliptic curve
nu1PointABasenu1I/OCrypto RAM3*u2ModLength + 12Input point A (projective coordinates)Resulting point C (projective coordinates)
nu1Workspacenu1ICrypto RAM4*u2ModLength + 28Corrupted workspace

Code Example

PUKCL_PARAM PUKCLParam;
PPUKCL_PARAM pvPUKCLParam = &PUKCLParam;


PUKCL (u2Option) = 0;

PUKCL _ZpEccDbl(nu1ModBase) = <Base of the ram location of P>; 
PUKCL _ZpEccDbl(u2ModLength) = <Byte length of P>;
PUKCL _ZpEccDbl(nu1CnsBase) = <Base of the ram location of Cns>;
PUKCL _ZpEccDbl(nu1PointABase) = <Base of the ram location of the A point>; 
PUKCL _ZpEccDbl(nu1ABase) = <Base of the a parameter of the elliptic curve>; 
PUKCL _ZpEccDbl(nu1Workspace) = <Base of the ram location of the workspace>;
...

// vPUKCL_Process() is a macro command, which populates the service name
// and then calls the library...
vPUKCL_Process(ZpEccDblFast,&PUKCLParam); 
if (PUKCL (u2Status) == PUKCL_OK)
            {
            ...
            }
else // Manage the error

Constraints

No overlapping between either input and output are allowed. The following conditions must be avoided to ensure that the service works correctly:

  • nu1ModBase, nu1CnsBase, nu1PointABase, nu1ABase, nu1Workspace are not aligned on 32-bit boundaries
  • {nu1ModBase, u2ModLength + 4}, {nu1CnsBase, u2ModLength + 8}, {nu1PointABase, 3*u2ModLength+ 12}, {nu1ABase, u2ModLength + 4}, {nu1Workspace, <WorkspaceLength>} are not in Crypto RAM
  • u2ModLength is either: < 12, > 0xffc or not a 32-bit length
  • All overlapping between {nu1ModBase, u2ModLength + 4}, {nu1CnsBase, u2ModLength +8}, {nu1PointABase, 3*u2ModLength + 12}, {nu1ABase, u2ModLength + 4} and {nu1Workspace, 4*u2ModLength + 28}

Status Returned Values

Returned StatusImportanceMeaning
PUKCL_OKThe computation passed without problem.