6 Configurations
The picture below presents the first interface the user encounters after adding the library to the project. The interface is comprised of the following elements:
- Resource Management Panel: The Resource Management Area has two views: The tree and flat views. Both provide access to the complete list of software/peripheral components and the selected components for the current project configuration.
- Application Builder Panel: A structured relationship manager with the used resources, providing a clear visualization of a component’s related dependencies and context in the project
- Composer Panel: When a peripheral, library or other external component is selected from the Project Resources area, its corresponding configuration GUI is displayed in the Composer area
- Pins Package Panel: Displays pins in graphical view and provides a zooming feature enabled by the scrolling mouse wheel when hovering with the cursor over the package view
- Pin Grid Panel: Displays pins in a structured table format, with lock and unlock features