5.6 Monitor ERPS
The ERPS Status page shows the status of the ERPS instances.Figure 5-17. ERPS Status

The ERPS Status page has the following parameters:
- ERPS #: The ID of the ERPS. Click on the link to get to ERPS detailed instance page, where you can reset counters and issue commands.
- Oper: The operational
state of ERPS instance
: Active
: Disabled or Internal error
- Warning: Operational
warnings of ERPS instance
: Active
: Disabled or Internal error
- State: Specifies protection/node state of ERPS
- TxRapsActive: Specifies whether we are currently supposed to be transmitting R-APS PDUs on our ring ports
- cFOPTo: Failure of Protocol:R-APS Rx Time Out
- Tx Information:
- UpdateTimeSecs: Time in seconds since boot that this structure was last updated
- Request: Request/state according to G.8032, table 10-3
- Version: Version of received/used R-APS Protocol. 0 means v1, 1 means v2, and so on
- Rb: RB (RPL blocked) bit of R-APS information. See figure 10-3 of G.8032.
- Dnf: DNF (Do Not Flush) bit of R-APS information. See figure 10-3 of G.8032.
- Bpr: BPR (Blocked Port Reference) of R-APS information. See figure 10-3 of G.8032.
- Node ID: Node ID of this request
- SMAC: The Source MAC address used in the request/state