5.14 Monitor PoE
The Monitor Power over Ethernet page allows the user to inspect the current status for all PoE ports.
The Monitor Power over Ethernet page has the following parameters:
- Local Ports: This is the logical port number for this row
- PD Class: Each PD is
classified according to a class that defines the maximum power used by the PD. The
PD Class shows the PDs class. The following classes are defined:
- Class 0: Max. power 15.4W
- Class 1: Max. power 4.0W
- Class 2: Max. power 7.0W
- Class 3: Max. power 15.4W
- Class 4: Max. power 30.0W
- Class 5: Max. power 45.0W
- Class 6: Max. power 60.0W
- Class 7: Max. power 70.0W
- Class 8: Max. power 90.0W
- Power Requested: Shows the requested amount of power the PD wants to be reserved
- Power Allocated: Shows the amount of power the switch has allocated for the PD
- Power Used: Shows how much power the PD currently is using
- Current Used: Shows how much current the PD currently is using
- Priority: Shows the port's priority configured by the user
- Port Status: The Port Status
shows the port's status. The status can be one of the following values:
- On: A PD is detected for the port
- ---: No PD detected for the port
- Not Supported: PoE not supported for the port
- Budget Exceeded: The total requested or used power by the PDs exceeds the maximum power the Power Supply can deliver, and port(s) with the lowest priority is/are powered down.
- Off: PD is off
- Disabled: User has disabled PoE for the port
- Shutdown: The port is shut down
- Overload: The PD has requested or used more power than the port can deliver and is powered down
- Unknown: PD detected but is not working correctly