5.15 Monitor MAC Table
Entries in the MAC table are shown on the MAC Address Table page. The MAC table contains up to 8192 entries and is sorted first by VLAN ID, then by MAC address. Each page shows up to 999 entries from the MAC table, default being 20, and selected through the entries per page input field. When first visited, this web page shows the first 20 entries from the beginning of the MAC table. The first displayed is one with the lowest VLAN ID and the lowest MAC address found in the MAC table.
The MAC Address Table page has the following parameters:
- Type: Indicates whether the entry is a static or a dynamic entry
- MAC Address: The MAC address of the entry
- VLAN: The VLAN ID of the entry
- Port Members: The ports that are members of the entry