9.11.3 boot
This attribute can be used to define protected variables in Boot Segment (BS) RAM:
int __attribute__((boot)) boot_dat[16];
Variables defined in BS RAM will not be initialized on startup.
Therefore all variables in BS RAM must be initialized using inline code. A diagnostic
will be reported if initial values are specified on a boot
variable.
An example of initialization is as follows:
int __attribute__((boot)) time = 0; /* not supported */
int __attribute__((boot)) time2;
void __attribute__((boot)) foo()
{
time2 = 55; /* initial value must be assigned explicitly */
}