GATTC_ReadUsingUUID
C
uint16_t GATTC_ReadUsingUUID(uint16_t connHandle, GATTC_ReadByTypeParams_T *p_readParams);Description
Initiates a read operation for a characteristic value by UUID within a handle range.
Note
This function starts a read operation for the value of a characteristic specified by UUID within the given handle range. The operation may result in a series of events indicating the status and results of the read operation.
Events generated
GATTC_EVT_ERROR_RESP indicates a failure to read the characteristic value.
GATTC_EVT_READ_USING_UUID_RESP indicates a successful read operation.
ATT_EVT_TIMEOUT indicates a timeout occurred because the server did not respond to the request.
Parameters
| Parameter | Description |
|---|---|
| [in] connHandle | Handle of the connection to read characteristic value for. |
| [in] p_readParams | Pointer to structure containing the UUID of the Characteristic and handle range to be queried. See GATTC_ReadByTypeParams_T. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Read operation successfully initiated. |
| MBA_RES_OOM | Memory allocation failure occurred internally. |
| MBA_RES_INVALID_PARA | Invalid parameters, such as an invalid connection handle. |
| MBA_RES_BUSY | GATT Client is busy with another ongoing request. |