GATTC_DiscoverAllDescriptors
C
uint16_t GATTC_DiscoverAllDescriptors(uint16_t connHandle, uint16_t startHandle, uint16_t endHandle);Description
Initiates the discovery of all descriptors with a specific UUID within a handle range.
Note
This function starts the discovery process for all descriptors with a specific UUID within the provided handle range. The discovery may result in a series of events indicating the status and results of the operation.
Events generated
GATTC_EVT_DISC_DESC_RESP with procedureStatus set to 'continue' indicates that one or more descriptors have been found, but the discovery process is ongoing.
GATTC_EVT_DISC_DESC_RESP with procedureStatus set to 'finish' indicates the end of the discovery process, either because the last descriptor has been found or no more descriptors are present within the range.
GATTC_EVT_ERROR_RESP with error code ATT_ERR_ATTRIBUTE_NOT_FOUND indicates the discovery process has ended due to no further descriptors being found.
ATT_EVT_TIMEOUT indicates a timeout occurred because the server did not respond to the request.
Parameters
| Parameter | Description |
|---|---|
| [in] connHandle | Handle of the connection to discover the descriptors for. |
| [in] startHandle | Start handle of the range to query. |
| [in] endHandle | End handle of the range to query. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully starts the discovering. |
| MBA_RES_OOM | Memory allocation failure occurred internally. |
| MBA_RES_INVALID_PARA | Invalid parameters, such as an invalid connection handle. |
| MBA_RES_BUSY | GATT Client is busy with another ongoing request. |