6.4 Erase Flash
Enables the bootloader to initiate erase commands to the memory driver.
Summary
This is the command to clear or reset memory values in the Flash portion of memory. An important note about this command is that the erase address must be aligned to the first address of an erase row. Any attempt to erase with an address not at the beginning of a row will be rejected with an address error code.