27.5.5 Master Status
Name: | MSTATUS |
Offset: | 0x05 |
Reset: | 0x00 |
Property: | - |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
RIF | WIF | CLKHOLD | RXACK | ARBLOST | BUSERR | BUSSTATE[1:0] | |||
Access | R/W | R/W | R/W | R | R/W | R/W | R/W | R/W | |
Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit 7 – RIF Read Interrupt Flag
This flag is set to ‘1
’ when the master byte read
operation is successfully completed.
The RIF flag can be used for a master read interrupt. More information can be found in the Read Interrupt Enable (RIEN) bit from the Master Control A (TWIn.MCTRLA) register.
This flag is automatically cleared when accessing several other TWI registers. The RIF flag can be cleared by choosing one of the following methods:
- Writing a ‘
1
’ to it. - Writing to the Master Address (TWIn.MADDR) register.
- Writing/Reading the Master Data (TWIn.MDATA) register.
- Writing to the Command (MCMD) bit field from the Master Control B (TWIn.MCTRLB) register.
Bit 6 – WIF Write Interrupt Flag
This flag is set to ‘1
’ when a master transmit
address or byte write operation is completed, regardless of the occurrence of a
bus error or arbitration lost condition.
The WIF flag can be used for a master write interrupt. More information can be found from the Write Interrupt Enable (WIEN) bit in the Master Control A (TWIn.MCTRLA) register.
This flag can be cleared by choosing one of the methods described for the RIF flag.
Bit 5 – CLKHOLD Clock Hold
When this bit is read as ‘1
’, it indicates that the
master is currently holding the SCL low, stretching the TWI clock period.
This bit can be cleared by choosing one of the methods described for the RIF flag.
Bit 4 – RXACK Received Acknowledge
When this flag is read as ‘0
’, it indicates that the
most recent Acknowledge bit from the slave was ACK and the slave is ready for
more data.
When this flag is read as ‘1
’, it indicates that the
most recent Acknowledge bit from the slave was NACK and the slave is not able to
or does not need to receive more data.
Bit 3 – ARBLOST Arbitration Lost
When this bit is read as ‘1
’, it indicates that the
master has lost arbitration. This can happen in one of the following cases:
- While transmitting a high data bit.
- While transmitting a NACK bit.
- While issuing a Start condition (S).
- While issuing a repeated Start (Sr).
This flag can be cleared by choosing one of the methods described for the RIF flag.
Bit 2 – BUSERR Bus Error
The BUSERR flag indicates that an illegal bus operation has occurred. An illegal bus operation is detected if a protocol violating the Start (S), repeated Start (Sr), or Stop (P) conditions is detected on the TWI bus lines. A Start condition directly followed by a Stop condition is one example of a protocol violation.
The BUSERR flag can be cleared by choosing one of the following methods:
- Writing a ‘
1
’ to it. - Writing to the Master Address (TWIn.MADDR) register.
The TWI bus error detector is part of the TWI Master circuitry. For
the bus errors to be detected, the TWI Master must be enabled (ENABLE bit in
TWIn.MCTRLA is ‘1
’), and the main clock frequency must be at
least four times the SCL frequency.
Bits 1:0 – BUSSTATE[1:0] Bus State
This bit field indicates the current TWI bus state.
Value | Name | Description |
---|---|---|
0x0 | UNKNOWN | Unknown bus state |
0x1 | IDLE | Idle bus state |
0x2 | OWNER | This TWI controls the bus |
0x3 | BUSY | Busy bus state |