OTA_SERVICE_Transport_RspRecv
C
uint32_t OTA_SERVICE_Transport_RspRecv(void* handle, char* buf, uint32_t bufSize)Summary
Read command response back.
Description
This function is used to read the response of RNBD for the command issued from host side.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| handle | Transport handle |
| buf | Expected response Buffer pointer |
| bufSize | Response buffer data size |
Returns
If we successfully receive the expected response message, the size of the message will be returned. However, in the event that we do not, the return value will be zero.
Remarks
None.