1.2.7 Using Range Operations
The range operation is similar to the equality operation, except that the constant field is a range of values instead of a single value. The check for bit equality is made for each constant value in the range.
First, define the address bus as follows:
FIELD address = [A3..A0]; |
Then write the RANGE equation:
select = address:[C..F]; |
This is equivalent to the following equation:
select = address:C # address:D # address:E #
address:F; |