1.2.4 Defining Logic Equations
[!] var [.ext] = exp; |
where:
|
var is a single variable or a list of indexed or non-indexed variables defined according to the rules for list notation. When a variable list is used, the expression is assigned to each variable in the list. .ext is an optional variable extension to assign a function to the major nodes inside programmable devices. exp is an expression; that is, a combination of variables and operators. = is the assignment operator; it assigns the value of an expression to a variable or set of variables. ! is the complement operator. |
In standard logic equations, normally only one expression is assigned to a variable. The APPEND statement enables multiple expressions to be assigned to a single variable. The APPENDed logic equation is logically ORed with the original equation for that variable. The format for using the APPEND statement is identical to defining a logic equation, except the keyword APPEND appears before the logic equation begins.
Place logic equations in the “Logic Equation” section of the source file provided by the template file.