2.1 Hardware Test Connection
Perform the following steps for the hardware test connection:
- Cut off the antenna path and solder the
RF coaxial cable on the RF test point.
Figure 2-1. RF Coaxial Cable Solder Test Connection on RF Test Point - Perform the following for test mode
connection (see the following figure):
- Connect the test interface of IS1870 DUT (VBAT, GND, HCI_TX, HCI_RX and P2_0) to Edgar III board (USB to UART Converter Board) (5V, BAT, GND, HTX, HRX and P2_0).
- Connect the Edgar III to the PC USB port.
- Connect the DUT to the RF tester.
- Set the P2_0 of SW1 to ON on Edgar III (P2_0 of DUT pulled to low).
Note: For more details, refer to Appendix B: Edgar III Circuit. Contact Microchip sales or an FAE for Edgar III boards.Figure 2-2. RF Test Mode Connection - Use the ISRT tool to configure the RF test parameter.
- Test with the RF equipment and verify the RF TX/RX performance.