6 Base Node Command Line Interface
The Linux application includes a Command Line Interface (CLI), which is useful to interact with the PRIME Network in real time. This section describes the different commands implemented. Consider all of this functionality as an example of an application for testing purposes and not as a definitive piece of software.
The command line includes a PRIME node accessible from the configuration menu for everything related with the PRIME network and other simple commands (like hostname, write, ping, ip,…) located on the generic nodes of CLI (show/enable/config).
CLI offers the possibility to save the configuration when any modification is finished running the following:
MCHP-PRIME-BASE> enable
MCHP-PRIME-BASE# configure terminal
MCHP-PRIME-BASE(config)#write memory
Configuration saved to /etc/config/prime.conf
To access specific PRIME commands, go to the PRIME node running the following:
MCHP-PRIME-BASE> enable
MCHP-PRIME-BASE# configure terminal
MCHP-PRIME-BASE(config)# prime
MCHP-PRIME-BASE(prime)#
Keying ‘?’ shows the specific commands for the PRIME node.
MCHP-PRIME-BASE(prime)#
config PRIME configuration
end End current mode and change to enable mode
exit Exit current mode and down to previous mode
fw-upgrade Firmware Upgrade
mac MAC Attribute
mlme PRIME MAC MLME Request Primitives
network PRIME Network
phy PRIME PHY PLME Request Primitives
pib PIB Attribute
reboot Reboot PRIME Modem
reset Reset
show Show PRIME
MCHP-PRIME-BASE(prime)#