6.2.1 Simple Code and Coverage Colors
No Color - No Coverage Data
Several C constructs do not generate executable code, so have no highlight. Examples shown above include:
- Preprocessor declarations -
#includestatements - Variable declarations and initializations
- Comments or commented out code
Green - Covered and Executed
Full coverage for a line occurs when the code on that line is executed completely.
The main() function executes and returns completely, so the
beginning, return and ending lines show full coverage.
The lines of the for loop are all executed to completion
except for the break statement, because the if
condition is never met. In loops and conditional statements, there are one or more
conditions or branches which must all be tested for full coverage.
Functions that are called and complete on a line, such as
calcAdd(), are fully covered.
Yellow - Partial Coverage
When code on a line is covered but only partially executed, this is considered partial coverage.
For the simple if statement, the evaluation of
a<b is executed but the assignment j=1 is not.
Therefore the line is partially covered. If the statements were on different lines, you
will see:
The if-else statement uses binary logic to determine the
branch condition. Because of the variable values chosen, the statement in only partially
covered because when a has a nonzero value, b will not
be evaluated.
Red - Covered but not Executed
As discussed above, in loops and conditional statements there are one or more conditions or branches which must all be tested for full coverage.
The if statement in the for loop is never
true, so the following break statement is not executed.
The condition of the if-else statement is evaluated so the
else branch is never selected and the following line with
calcSub() is not executed.