3.3.2 Fitness Tracker Application on SAM D21 Curiosity Nano Evaluation Kit and Nano Base for Click Boards
Description
The application demonstrates a solution based on Microchip products for health care industry and wearable products. The application displays heart rate readings (in beats per minute - bpm) on a very low power consuming display. The Mikroelektronika Heart Rate 9 click board is used to read the heart pulse. Mikroelektronika Eink E-Paper display 2,9" 296x128 dots display is used for displaying heart rate.
The Eink E-Paper display 2,9" 296x128 dots display contains the eINK click adapter board and the E-Paper display 2,9" 296x128 dots display.
The Heart Rate 9 click introduces Microchip's proprietary method of measuring multiple signals in a body using pseudorandom binary sequence generation and phase division multiplexing This algorithm for processing data from the sensor and it can send data for 3 different diodes (green, ir, red) who give out a diagram of the heartbeat and its frequency per minute.
The Eink E-Paper display 2,9" 296x128 dots display is a very low power consumption display and it can retain the information, even after disconnecting from the power source. The host MCU SAM D21 is interfaced with the
Heart Rate 9 click over the USART interface and eINK click over SPI Interface.
Modules/Technology Used
- Peripheral Modules
- Timer
- EIC
- SERCOM (SPI)
- SERCOM (USART)
- STDIO Library
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/sam_d21_cnano.
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Mount SAM D21 Curiosity Nano Evaluation Kit on "CNANO56_HOST_CONN"(U3) connector of Curiosity Nano Base board.
- Mount Heart Rate 3 click board on mikro bus click 3 connector of Curiosity Nano Base board.
- Mount the Eink E-Paper display 2,9" 296x128 dots display (eINK click + E-Paper display 2,9" 296x128 dots Display) on the mikro bus 1 connector of Curiosity Nano Base board.
- Power the SAM D21 Curiosity Nano
Evaluation Kit from a Host PC through a Type-A male to Micro-B USB cable connected to
Micro-B port (J105).
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File.
- In the Import Image File
window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file.
- Select Device as ATSAMD21G17D.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Programming/Debugging Application Project
- Open the project (fitness_tracker\firmware\sam_d21_cnano.X) in MPLAB X IDE
- Ensure SAM D21 Curiosity Nano is selected as hardware tool to program/debug the application
- Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Demo
- Perform a reset by unplugging and re-plugging the power cable of SAM D21 Curiosity Nano Evaluation Kit.
- After power up, the application displays the "microchip logo" on the Eink E-Paper display 2,9" 296x128 dots Display and initializes the heart rate sensor.
- After successful initialization, keep
the finger on Pulse Detection Indicator on the heart rate 9 click sensor as shown in
the figure below.
Note: Place the index finger gently on the heart rate 9 click sensor as shown in the above figure. - Press switch "SW0" on SAM D21 Curiosity Nano Evaluation Kit, LED "LED0" on SAM D21 Curiosity Nano Evaluation Kit glows on.
- Wait till the LED "LED0" on SAM D21 Curiosity Nano Evaluation Kit goes off and then lift the finger.
- The heart rate value (in bpm - beats
per minute) gets displayed on the Eink E-Paper display 2,9" 296x128 dots Display.
Comments
- Place the index finger gently on the heart rate 3 click sensor, do not push or put pressure on the sensor (the heart rate values may not be accurate).
- Reference Training Module:
- This application demo builds and
works out of box by following the instructions above in Running the Demo
section. If the user needs to enhance/customize this application demo, should use the
MPLAB Harmony v3 Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- MPLAB Harmony v3 is configurable through MPLAB Code Configurator (MCC). Refer to the below links for specific instructions to use MPLAB Harmony v3 with MCC.