6.2.5.12 RLM System Info
If you select System Info from the menu on the left, you will see the RLM system information screen below in the view area. This information contains the platform type and hostid information for the system where the rlm process is running (NOTE: not where your browser is running). In addition, this screen will display a list of all rlm processes running on this computer (including processes which are not currently running but which have run in the prior 24 hours).