6.2.5.3 Main Status screen
If you select Status from the menu on the left, the main status screen is displayed in the view area as shown below. The top section displays the host information where the rlm server is running - host name and port #. Below this is status of the RLM server itself, followed by buttons to edit rlm options and display the last few lines of the rlm debug log.
Next is a table of ISV servers, one per line, with a number of buttons on the right-hand side of each line to retrieve ISV server status, license status, display the last few lines of the debug log, reread or restart the server, edit server options, or shut down the ISV server. Note that these buttons (and the corresponding columns) will only appear if the user running the web server has access to these functions, as specified in the rlm options file.
The status screen provides access to the shutdown and reread/restart commands for all the ISV servers, as well as option file editing and debug log viewing for both rlm and the ISV servers.