6.4.1.14 RLM_ROAM

RLM_ROAM controls license roaming operations. If RLM_ROAM is set to a positive integer N, subsequent checkout requests will attempt to create roaming licenses for N days. If RLM_ROAM is set to any negative integer, any subsequent license checkouts will cause a roaming license to be returned to the floating license pool. This last operation must be done when connected to the network such that the original license server can be contacted.

Setting RLM_ROAM disables RLM_QUEUE (starting in RLM v12.0).