6.2.6.3 ACTIVATE
ACTIVATE [off | url URL | isv ISVNAME]
The ACTIVATE line allows you to set the defaults for the URL and ISV name for activation.
The 2 forms of the ACTIVATE line are:
- ACTIVATE url URL
- ACTIVATE isv ISVNAME
In the first form “URL” is the default URL used for activation. For example:
ACTIVATE url www.reprisesoftware.com
In the second form “ISVNAME” is the default ISV name used for activation. For example:
ACTIVATE isv reprise
Note: In v15.2 and earlier a third form was available (ACTIVATE off).
Activation is now restricted to user with Manage or Admin roles.