GPD transmits the data packet to the sink device via proxy, if the proxy device is
present in the network. In such cases, the proxy device sends the GP notification on
behalf of the GPD device. The following figure illustrates the data transmission from
the GPD via proxy.Figure 8-4. Data Transmission from GPD via
Proxy
If the proxy device is not present in the network, the GPD sends the data to the sink
device. The following figure illustrates the GPD data TX without proxy.Figure 8-5. GPD Data TX Without
Proxy