50.6.5.3.2 Application Example
The figure below illustrates an application example of the Cycle-by-cycle Duty mode.
In an LED string control circuit, Cycle-by-cycle Duty mode can be used to automatically limit the current in the LED string.
The figure below illustrates an application example of the Cycle-by-cycle Duty mode.
In an LED string control circuit, Cycle-by-cycle Duty mode can be used to automatically limit the current in the LED string.
DS60001825G
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.