37.5.9 Comparison Window

The ADC Controller features automatic comparison functions. It compares converted values to a low threshold, a high threshold or both, depending on the value of ADC_EMR.CMPMODE. The comparison can be done on all channels or only on the channel specified in ADC_EMR.CMPSEL. To compare all channels, ADC_EMR.CMPALL must be set.

If set, ADC_EMR.CMPTYPE can be used to discard all conversion results that do not match the comparison conditions. Once a conversion result matches the comparison conditions, all the subsequent conversion results are stored in ADC_LCDR (even if these results do not meet the comparison conditions). Setting ADC_CR.CMPRST immediately stops the conversion result storage until the next comparison match.

If ADC_EMR.CMPTYPE is cleared, all conversions are stored in ADC_LCDR. Only the conversions that match the comparison conditions trigger the ADC_ISR.COMPE flag.

Moreover, a filtering option can be set by writing the number of consecutive comparison matches needed to raise the flag. This number can be written and read in ADC_EMR.CMPFILTER. The filtering option is dedicated to reinforcing the detection of an analog signal exceeding a predefined threshold. The filter is cleared as soon as ADC_ISR is read, so this filtering function must be used with the DMA controller and works only when using Interrupt mode (no polling).

The flag can be read on ADC_ISR.COMPE and can trigger an interrupt.

The high threshold and the low threshold can be read/write in the Compare Window register (ADC_CWR).

Depending on the sign of the conversion, chosen with ADC_EMR.SIGNMODE, the high threshold and low threshold values must be signed or unsigned to maintain consistency during the comparison. If the conversion is signed, both thresholds must also be signed; if the conversion is unsigned, both thresholds must be unsigned. If comparison occurs on all channels, SIGNMODE must be set to ALL_UNSIGNED or ALL_SIGNED and the thresholds must be set accordingly.