2.2.1 ECDH Command
The ECDH command has been updated to allow the selection of the source
private key location and target the premaster secret key location. The two possible
sources for the private key location are the TempKey and the EEPROM key slot. The target
premaster key location can have any of the following locations: output buffer, EEPROM or
TempKey.
When the Encrypted mode is selected by the ECDH command, the
output premaster secret is encrypted using the I/O protection key.