11.1.2.4 Adding custom Project Properties
The Project Properties dialog in autoload.py can display a custom JPanel ,
created using Java Swing objects from within jython.
- To enable MPLAB X IDE to discover the new JPanel, autoload.py must
contain a function called
mplab_configure_XXXXXXX, whereXXXXXXis a user-defined string of characters:. An entry namedXXXXXXXwill show up under the configuration node of the Project Properties. - If
present,
save_mplab_configure_XXXXXXis called when the user closes the Project Properties dialog or presses Apply. At this time, the script should read user input from the Java Swing objects and save them to the settings object usingsettings.setString().
Example
def mplab_configure_Bootstrap(confName):
global bsOpt
if bsOpt == None:
bsOpt=BootstrapPane()
return bsOpt.getPanel()
def save_mplab_configure_Bootstrap(confName):
global bsOpt
if bsOpt == None:
return
settings.setString("boot.path", bsOpt.binTxt.getText())
settings.setString("boot.prj", bsOpt.prjTxt.getText())
settings.setString("boot.load_adr", bsOpt.loadTxt.getText())
settings.setString("boot.entry_adr", bsOpt.entryTxt.getText())
settings.setString("boot.use", "true" if bsOpt.useBs.isSelected() else "false")For a complete example, look in the j-link_cortex-a5.py file in the IDE pack folder . This script creates and declares a Bootstrap pane for MPU projects.