12.5.3 Couldn’t reserve space for heap (Windows® OS)
MPLAB X IDE uses the MinGW in its make process. In Windows OS, you may have virtual memory allocation issues while GNU make is running.
Windows 7 or 8
To change the Virtual Memory settings, click . Then click System and then . On the Advanced tab, click on the Performance Settings button. In this dialog click the Advanced tab and then click on the Change button. Enter a custom size value as follows:
- Initial Size (MB) = Currently Allocated (shown at the bottom)
- Maximum Size (MB) = Recommended (shown at the bottom)
Click Set, click OK, and reboot your personal computer.
Windows 10
See:
www.geeksinphoenix.com/blog/post/2016/05/10/how-to-manage-windows-10-virtual-memory.aspx