12.5.7 Hexmate Conflict Report Address Error
When Hexmate generates a conflict report, the address of the conflict in the hex file is sometimes not the same as the address shown in a memory window (where the data resides in memory.) For example:
| Device Family | Address in Hex File | Address in Memory |
|---|---|---|
| Baseline | 0x100 | 0x80* |
| Midrange | 0x100 | 0x80* |
| PIC18 MCUs | 0x100 | 0x100 |
| 16-bit Devices | 0x100 | 0x80* |
| 32-bit Devices | 0x100 | 0x100 |
| * For some devices, the address shown in the conflict report is twice as large as the address of the data in memory. | ||
For more information on using Hexmate, see MPLAB XC8 documentation or Hexmate User’s Guide (DS-50003033) on the Microchip website.