7.4 Editor Red Bangs
The Editor highlights syntax and semantic errors,
such as missing semicolons and unresolved identifiers, in your source code. Errors are
shown in red underline and a red bang “glyph”
is displayed
in the left margin of the editor window next to each line that contains an error. An error
message is displayed when you mouse over the glyph.
Error Conditions and Additional Marking
Errors may occur when you do one of the following:
- Type in new code
- Edit existing code
- Add an existing file to your project
- Move a file to a different location in your project
- Change the properties of the project or one of its source files
If there are any errors in a file, red marks are displayed in the error stripe on the right side of the editor window. The error stripe represents the whole file, not just the lines currently displayed. Double click a mark in the error stripe to jump to the line the mark represents.
Errors Caused by Unrecognized Symbols
A symbol that is unrecognized by a compiler preparser or parser could be marked as an error but may not actually be an error (the code will build). Therefore, if you suspect this type of error, try to build the project anyway.
For examples, see the following issued under Errors:
- For 8-bit code,
#asmand#endasmcause red bangs in the Editor window. - For 16-bit code, MPLAB XC16
packedattribute statement causes red bangs in the Editor window. - For DSC code, MPLAB XC-DSC
packedattribute statement causes red bangs in the Editor window.