9.6.3 Configuration
You must specify a block of memory in SRAM for the Micro Trace Buffer (MTB.) The block must be minimum 128 bytes.
Using the Buffer combo box, you can either:
- choose a global variable from the
drop-down menu (e.g.,
volatile int buff[128];)
- specify the start address and size in
the format of
address;size(e.g., 0x2000000;0x100)
If you do not configure the buffer correctly (e.g., if the specified memory block is outside of SRAM memory range or the size does not meet the minimum size requirement), a message dialog will pop up when you start MTB.
In the Mode combo box, you can select what to do when the MTB is full: Auto halt debugger, Auto stop trace, or Overwrite old data.